This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS7A33: Positive and negative LDO can't power on Synchronously

Part Number: TPS7A33
Other Parts Discussed in Thread: TPS7A47,

hello, 

I used TPS7a4700  and TPS7A3301 to supplied ±18V for my audio amplifier TME49724 。 At powering on, the amplifier outputed a pulse voltage (tens of  milliseconds,up to 8V) ,which damaged my audio ADC。 I suspect that negative and positive power sources have different ramp time that leads to this problem.According to waveform captured,+18 voltage  can  power on in  a  few milliseconds, but -18V takes hundreds of milliseconds .So, is there any suggestions can solve this problem ?

Besides, the capacitors added the two LDO ss/nr pins are 1uF。