This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV62585: setting a minimum Vin by EN pin

Part Number: TLV62585

Hello everyone,

I'm developing a li-ion battery circuit using TLV62585 and I want to define a minimum input voltage of 3.2V, because in the battery data sheet the minimum voltage is 2.7V and the UVLO of TLV62585 is 2.45V (max). Is it possible to set a minimum Vin of 3.2V using a voltage divider on the EN pin? If so, can the bias current change the divider voltage?

Thanks!