Hi team,
Could TPS92611-Q1 output pin(Vout) pass the ESD Test Levels (IEC/EN 61000-4-2) Level 4 (contact:8kV and air:15kV?)
Regards,
Roy
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi team,
Could TPS92611-Q1 output pin(Vout) pass the ESD Test Levels (IEC/EN 61000-4-2) Level 4 (contact:8kV and air:15kV?)
Regards,
Roy
Hi Frank,
I review some data in internet, I see IEC6100-4-2 is system level ESD spec, and HBM/CDM is chip level ESD spec.
Does it mean we couldn't promise that our IC could pass the system level ESD spec?
Roy
That's a sysrem level standard and you can add other componet like ESD diode to help customer's system pass the level, and if that the same question as other question i will close this topic