Hi Experts
My customer has the following questions about this device:
Section 8.2.2.1 Selecting the Switching Frequency (page 30)
- “Equation 8 and Equation 9 must be used to find the maximum switching frequency for the regulator, choose the lower value of the two equations. Switching frequencies higher than these values result in pulse skipping or the lack of overcurrent protection during a short circuit.”
Does this mean that setting the shifting frequency to a value above Equation 8 (max skip) forces the regulator into pulse skipping eco-mode (PSM)?
Section 8.2.2.11 Discontinuous Mode and Eco-mode Boundary (page 35).
- Output current of 5mA listed as the boundary between discontinuous conduction mode (DCM) and pulse skipping eco-mode (PSM)
- Output current of 337mA listed as the boundary between continuous conduction mode (CCM) and discontinuous conduction mode (DCM)
I know these values are specific to the design example. Are there formulas to calculate these boundary values in general?
Thanks for your help.
Best regards,
Jim B