Hello there,
I found a previous thread somewhat helpful as it clarified that the TPS7A45XX has current limiting protection which limits the output current depending on Input-Output differential voltage and ambient free air temperature, and is not based solely on junction temperature.
Previous thread: https://e2e.ti.com/support/power-management/f/196/p/698922/2582061#2582061?jktype=e2e
I am left with two questions:
1. What is meant by "T_A - free air temperature" in figures 20 and 21 of the TPS7A45XX datasheet (included below)? As the package heats up during operation, am I to assume that the current-limiting circuitry is responding to a bulk air reservoir temperature and is isolated from the heating of the package? Is there a more precise definition that can help me understand the relationship between the current limit and the junction and/or package temperature?
2. Several responses to 'thermal protection' and 'current limit' questions infer or state that the current limiting circuitry, while not primarily dependent upon, is still affected by how the part is heat sunk. In my application, the TPS7A4501KTTR (DDPAK) is mounted such that it has a conductive thermal path with resistance of <5°C/W from its junction to an external reservoir. In this instance, based on the responses in the thread linked above, I expect the current will not be limited by junction temperature or the amount of power I can dissipate in the package. I would like to understand what I can expect the output current to be limited at given a much lower junction-ambient thermal resistance than figures 20 & 21 are supposedly generated from.
Any help you can offer will be greatly appreciated. I plan on conducting a test regardless, but I would like to understand this better beyond any empirical measurement.