Other Parts Discussed in Thread: TPS62743
Hello,
I'm looking through a few options for a step-down converter (3.6V to 1.2V) and I'm a bit puzzled by the datasheet graphs for the TPS62746. This converter seems to be designed specifically to give 1.2 or 1.8V outputs, yet efficiency curves are shown for various voltages from 0.8V to 3.3V. These curves also refer to the wrong part number (they say TPS62743) so it looks like these are copied from anther datasheet and haven't been replaced with the correct data.
Is the correct efficiency data available for this part, for 1.2V and 1.8V outputs?
Thanks,
Gordon.