Hello,
About the enable pin of the DC-DC lMZ12002, in the "absolute maximum ratings" part the maximum voltage allowed is V_(EN MAX) = 7V but in another part of the datasheet it is described that is possible to leave pin enable floating for always-on operation, the problem that for this configuration the EN pin is internally pulled up to VIN. and for information, Vin is can be raised to 20 V exceeds V_(EN MAX). It's not contradictory?