Other Parts Discussed in Thread: TPS731
Dear Team,
I understand that TPS793 is a product that features the fast start-up.
However, I would like to delay the rise time as a measure against inrush current.
Looking at " 6.5 Electrical Characteristics " of the datasheet, I think the start-up time can be delayed by increasing CNR.
Is it OK to increase the CNR to the maximum ? If so, what is the expected start-up time ?
I think that the operation will be affected if the capacity is large.
The required specifications are as follows.
Vin=4.8V
Vout=4.6V
Iout=20mA to 30mA
inrush current=200mA or less
Sincerely,