Hello TI,
we developed a QI-transmitter based on the BQ500410A with the MSP430. We set the LEDs to option 1 (Generic) with a 42.2 k 1% resistor. Additionally we added a yellow LED to the 3v3 as a standby. Most of the time we see the described reaction of the LEDs (charging is green slow blinking, charge complete is green on and fault is red on and PMOD or FOD is red fast blinking).
But this behaviour does not stay active all the time. Sometimes the green LED shortly blinks which i assume is a new communication start to check if still full, This would be acceptable but in some cases after this short blink the green LED does not return to the on state and stays off. The battery was not moved and the QI-transmitter is all the time powered which can be seen by the yellow standby LED we added.
Any suggestions on how to fix this issue?
Kind regards,
Carsten Lechens