This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5575-Q1: ---

Part Number: LM5575-Q1
Other Parts Discussed in Thread: LM5575

Hi,

   About the chip LM5575-Q1, I have some question. At the moment of 24V power on, the chip have a 8V peak voltage ,about 10ms, but it should be 5V. When I change the ceramic capacitor C48 from 100nF to 10nF, it become normal. I want to know the reason. Give me a hand ,thanks.

   The attachment is my sch and layout.资料.zip