Other Parts Discussed in Thread: TL432
Hello guys,
One of my customers is trying to use TL431 for their new products.
The have a few questions as the follows.
Could you please give me your reply?
Q. The customer is trying to understand the following document.
Understanding Stability Boundary Conditions Charts in TL431, TL432 Data Sheet (SLVA482A)
They have a few questions at Figure 5, ESRs @ Vka=2.5V graph.
(1) They think this graph shows the minimum ESR of capacitance attached between the both terminal of TL431 for stable output voltage as a shunt regulator.
Also Figure 1 in this document says output voltage is stable when 0.01uF is connected to TL431. But Figure 5 says the capacitor minimum ESR need to be 20~50ohm at the capacitance value.
They think 20~50ohm ESR is very big and it is not reasonable. The Figure 5 is correct?
(2) If figure 5 is correct, 20~50ohm resistor must be connect to the capacitor in series when the capaciance is 0.01uF?
(3) ESR of capacitor changes due to frequency. Which frequency the ESR which Figure 5 says at?
Your reply would be much appreciated.
Best regards,
Kazuya.