Other Parts Discussed in Thread: TPS22810
Hi, I have been looking for a load side switch and came across the TPS22934 and it seems to be what I am looking for.
I have a Capacitor that is rated at 3V and I want to discharge it to the load when it's almost full around 2.6V. Is that possible with this load switch?
I am not understanding the datasheet too much. It says it has a hystererisis input of 2.35. So does this mean when the enable pin gets 2.35 V the switch will close and let the voltage flow through to the load?
Is there an under voltage where it detects low voltage around 0.9V to open the switch to disconnect from the load?