Other Parts Discussed in Thread: TPSM53603, TPSM53604, LMZM23601
Hi
Can i use TPSM84205 for -5V output?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi PY,
I think the LMZM23601 configured for IBB may be the better option out of the two devices simply because of it's size. The LMZM23601 is 3.8mm x 3mm device and can be used in your power application of 8V-27V (typical 12Vin) /-5Vout and 12Vin/-12Vout at 300mA loading.
Regards,
Jimmy