This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC3817: Can be reached to input frequency up to 440 Hz for UCC3817?

Part Number: UCC3817
Other Parts Discussed in Thread: UCC381,

Hi E2E

A new project for industrial application with 300W output.

1. AC line input frequency from 40Hz to 440Hz.
2. AC line input voltage from 90Vac to 265Vac.
3. PF need 0.98 at 230Vac/440Hz

Therefore, I need to have this kind of PFC controller to fulfill customer requirements.

 

Can UCC381 can reach this design or another IC? 

Best regards,

Rock Shao