This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5060: UVLO & Schematic review

Part Number: LM5060
Other Parts Discussed in Thread: LM25119, LM5069

HI

1. Have used tool to do calculations, and later got a set value table,
    Because the lowest voltage actually measured at present cannot be turned on at 8.4V,
    It is a bit different from the cognitive Lower UVLO = 7.59V.
    Therefore, I would like to ask which value should I look at for overvoltage and undervoltage protection? Upper or Lower?

2.Does Typical Over-Current Threshold mean the OCP threshold at the lowest voltage?

3.Please kindly help us to check the schematic , LM5060 & LM25119

C6939_B_SCH_PWRIN.PDF