Hi,
It's seem like no difference while I test the TPS53316—EVM both DCM and CCM @ same load, the curve and switching frequency is the same.
So how to understand "In HEF, PWM modulator determines the switching frequency" that show in the datasheet?
and which application should choose DE mode? when HEF mode?
Best regards
Thank you.
CH1: Vsw CH3:Vo CH4:Io(DE mode 0.5A load) |
CH1: Vsw CH3:Vo CH4:Io(HEF mode 0.5A load) |
CH1: Vsw CH3:Vo CH4:Io (DE mode 5A load) |
CH1: Vsw CH3:Vo CH4:Io(HEF mode 5Aload)
|