This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Champs,
A customer would like to know whether "Fusion Digital Power Studio" could control the functions with UCD3138ALLCEVM150 as follows:
1)Synchronous rectification control. control the driver for UCD7138.
2)Over current and voltage drop detection, and Trip which stops PWM and automatically recover.
3)Over voltage detection.
4)Soft-Start time control. they would like to change the time.
5)Burst control with no load or light load.
6)the resolution change for PFM switching
7)Dead time resolution and accuracy
I would very appreciate if you could let us know which items from 1) to 7) can be controlled by "Fusion Digital Power Studio."
Thank you for your kind support.
Best regards,
Hitoshi
Hello, open Fusion Digital Power Studio, click "Configure" in the left bottom corner, it shows all the parameters you can configure from the GUI. If the parameter you want to change is not there, then you need to modify the firmware.
Hi Bosheng,
If "Fusion Digital Power Studio" does not support the requested items, is it possible to use UCD3138FW_LLC which is the CCS project file?
Thank you for you kind check.
Best regards,
Hitoshi
Hi Hitoshi: Yes, you can download the UCD3138FW_LLC code, then modify or add whatever features you want.