Hi Sir,
Would you pls advise 2 questions as below?
1. For Hiccup mode, check with d/s, it means overload protection.
It will calculate PWM clock cycles if >64 cycles, it will turn off switching and pulls down SS
Woud you pls kindly etail describe?
2. Standby mode looks only between start up and run mode?
If any way can enter standby mode?
3. If system want to control LM51551-Q1 by SOC.
If it mean connect as below,
When SOC pull high 3.3V > UVLO threshold 1.5V, enter run mode; pull low is shut down?
Thanks, Ian.