Part Number: BQ78350-R2-DEVICE-FW
Hi Team,
My customer is testing CB in bq78350-R2. There are some interesting investigate and need your comment to clarify. Btw, this is 10S application.
Here is CB setting for your reference.
- Cell Balance Threshold : 3800
- Cell Balance Window:100
- Cell Balance Min:15
- Cell Balance Interval:5
Test Method and Result
- Using power supply to charge cell #3 , #6 ,# 8 to cause their cell voltage is higher 50mV than ones.
- Charging to whole system with different “Cell balance window ”setting – 100mV,50mV , Logging by bqStudo to observe the changing.
Attached #1 – Cell balance window = 100mV --> By checking CB in operation status B, we notice CB is activated in the beginning , however it stop balance after 1 min even if the deltaV is higher 50mV
Attached #2 – Cell balance window = 50mV --> We saw the cell#5 voltage is changing a lot.
Could you kindly take a look this symptom?