This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS7A7200: Power management forum

Part Number: TPS7A7200
  1. Want to know when  Power Good  is goes  high, whether it is at input supply or at the when enable is active.

 

  1. And what is the state of PG which is pulled high with 2.5v before enable is active   for  TPS7A7200

  • HI Dilip,

    To answer your questions:

    1. PG goes high when VOUT is >90% of the VOUT target. Meaning if VOUT is 3.3V, PG will assert above ~2.97V. 

    2. As long as VIN is above 1.425V, the internal circuitry is up and running. So PG is held low until VOUT rises above the PG threshold. 

    I hope this answers your questions