Other Parts Discussed in Thread: TPS61089, TPS55288, TPS61022
Hello,
TPS61089EVM-742 output change to 5.25V.(R1=1M, R2=300k)
VIN=5.5V drive,
Q1. 1st output is 6.0V overshoot.(see attached PDF Fig.1)
I want to start non overshoot.
Q2. VOUT conected E-load. Load is 0.0A to 3.0A ramp.
VIN current measurement spike wave and VOUT big ripple.(Fig.2)
3.0A load, SW pin operate mode DCM? PFM? strange behavior.(Fig.3)
Is there any way to improve on these issues?