Dear the person in charge of BQ24171EVM-706-15V,
I have a question.
It is written as below for the subject "2.7.4 Charger Termination and Recharge" of bq24171EVM user's guide(SLUU462A–November 2010–Revised February 2011).
>Increase the voltage of LOAD#2 slowly to approximately 4.2 V for 001 and 12.6 V for 002 / 003.
>Observe → I(J2(VBAT)) decreases from 2 A while V(J2(VBAT)) becomes constant.
>Observe → I(J2(VBAT)) drops to zero when LOAD#2 current is less than 0.2 A.
When I(J2(VBAT)) droped to zero, how does LED D1 state become?
(blink or OFF or ON?
Could you tell me for the above?
Best regards,
Hiroyuki