Other Parts Discussed in Thread: UC3823, UC3823B
Hi Team,
Could any expert help to check if we have any temp related characterization data for pin 9?
Etther UC3823/UC3823A/UC3823B is ok.
Customer is asking, thanks!
Andrew
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I will check and reply to you
ILIM: 0-degree C to 70-degree C
* current limit threshold ICL, 0.95V to 1.05V
* over current limit threshold ICL, 1.14V to 1.26V
Hi Hong,
Thanks for quick help!
So is the temp-co like -> current limit threshold ICL, (0.95V to 1.05V), is this meaning (1.05-0.95) / 70C = 0.001429/C ?
Thanks!
Andrew
Also, individual devices may have smaller variations and different from part to part. The specs are covering all possible range for this device.
No, we do not have graph data. The specs are based on a number of units test and then using statistical methods to decide the specs.