This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I would appreciate your review of the attached schematic and comments/answers to the following details that arose during the design process.
i. Pack’s circuit disconnects cell first, BQ25616 has no voltage source so at VAC/VBUS or BATT pins so it goes dark and cannot further effect pack until charger is plugged in.
ii. BQ25616 circuit disconnects cell first above pack’s 2.3 V trip off point, as per datasheet section 9.3.9.5.2 Battery Over-Discharge Protection. While pack supplies voltage to BATT pins the BQ25616’s Iq_bat quiescent battery current of circa 9.5 uA remains as a load on the pack. Thus eventually that uA load along with the cell’s self-discharge will eventually reach the pack’s 2.3 V trip off point. Stability depends on BQ25616 keeping battery disconnected from load as voltage on BATT lingers between 2.62 and 2.3 VDC.
5. Datasheet sections 10.2.1.2.1 Inductor Selection, 10.2.1.2.2 Input Capacitor and Resistor, and 10.2.1.2.3 Output Capacitor all use formulas that are a function of the switching frequency duty cycle. Prior to building a circuit and bench testing how is the duty cycle to be known? WEBBENCH or Tini-TI models do not appear to be available for simulation. Failing that the values used in datasheet and BQ25616EVM schematics were used. Are these sufficient or should they be checked against some range of duty cycles? If so what % range of 1.5MHz?
I would appreciate your review of the attached schematic and comments/answers to the following details that arose during the design process.
Yes, D+/D- floating as unknown adaptor so that ILIM pin can limit input current.
Yes, correct.
Yes, correct.
Yes, correct if VBUS is not attached. If with VBUS attached, VBAT_DPL is not used, and the charger operates in charge mode.
Given the pack’s protection circuit cutoff voltage is within the range of BQ25616’s VBAT_DPL is there a danger the two circuits will trip each other into misbehaving? With no voltage present on VAC/VBUS pins two scenarios as battery reaches discharge state come to mind.
Battery pack and protection and BATFET pin the charger are in series, which ever is triggered first, SYS is disconnected from battery, there is no conflict between the two.
i. Pack’s circuit disconnects cell first, BQ25616 has no voltage source so at VAC/VBUS or BATT pins so it goes dark and cannot further effect pack until charger is plugged in.
Yes, correct.
ii. BQ25616 circuit disconnects cell first above pack’s 2.3 V trip off point, as per datasheet section 9.3.9.5.2 Battery Over-Discharge Protection. While pack supplies voltage to BATT pins the BQ25616’s Iq_bat quiescent battery current of circa 9.5 uA remains as a load on the pack. Thus eventually that uA load along with the cell’s self-discharge will eventually reach the pack’s 2.3 V trip off point. Stability depends on BQ25616 keeping battery disconnected from load as voltage on BATT lingers between 2.62 and 2.3 VDC.
I agree with your analysis. The 9.5uA should be 6.5uA because BATFET is off.
5. Datasheet sections 10.2.1.2.1 Inductor Selection, 10.2.1.2.2 Input Capacitor and Resistor, and 10.2.1.2.3 Output Capacitor all use formulas that are a function of the switching frequency duty cycle. Prior to building a circuit and bench testing how is the duty cycle to be known? WEBBENCH or Tini-TI models do not appear to be available for simulation. Failing that the values used in datasheet and BQ25616EVM schematics were used. Are these sufficient or should they be checked against some range of duty cycles? If so what % range of 1.5MHz?\
Your schematic values look good. No further calculation is needed.
Thanks for your quick response Hong Mao. It really helps to get a design to production with minimum revisions.