Hi,
I would like to ask you about the UCC28950 device.
I am creating a circuit asynchronously.
(question 1)
DCM mode begins when the voltage on the CS pin falls below a user-set threshold and OUTE and OUTF go low in the data sheet.
However, since I am creating the circuit asynchronously, what is the behavior in this case?
(Question 2)
I don't think the DELEF and ADELEF settings are required for asynchronous circuits. In this case, what kind of settings should these pins have?
Can these pins be open?
(Question 3)
The sink and source currents of OUTA, OUTB, OUTC, and OUTD are specified as electrical characteristics of 0.2 A (TYP).
Is there a maximum rating for these sink and source currents?
Best regards,