Other Parts Discussed in Thread: UCD90SEQ48EVM-560
This is an urgent request.
I have a customer using the UCD90SEQ48EVM-560 that has a socket, to allow for UCD9090A devices to be swapped in/out and programmed with the same basic setup.
They programmed two devices using the same setup, and the same *.fifsp file, but are seeing a discrepancy in the data between the two devices in the following address:
address-hex: 0000018D20~0000018E70
1. What is stored here at these address values?
2. Is it okay for these values to be different for different devices over process, if the same program is written?
Thanks,
Darren