Other Parts Discussed in Thread: LM5161, LM5164
Hi Team
My customer is using LM5160 to provide 18V to the application.
Due to some confidential information, I'll write the application in thread tracking toolkit.
External supply voltage to LM5160 will be DC48V, the customer wants to know how LM5160 would behave if external supply
voltage exceeds LM5160's Vin(max), 70V.
He is asking this because he worries if the voltage will also be applied into the application and cause destruction inside the
application.
Thanks.