Other Parts Discussed in Thread: ISO5452
Tool/software: WEBENCH® Design Tools
Hello,
Need your immediate support
I downloaded unencrypted spice model of ISO5852SDW for ISO5452. I am working in Simetrix which can support this Spice model.
1.) I could not observe Desat Protection under 5 Us.
2.) I cannot see the soft shutdown during desat.
I ran multiple times and rechecked everything, Would like to know if I need any modification in my Circuit for simulation or The spice model which I am using is not complete ?
Below waveforms for your reference.
Please note the C-E Voltage (Second curve) is maintained at 10 V after 100 Us for desat
Third Curve shows the G-E voltage, Would like to mention that there is no soft turn off. .. Turned off and Turned again even after C-E (10 V) is detected...The turn off time is also higher than 5 Us from Desat moment (although it is not shown in below pic)
The Fourth Curve shows the Desat Voltage.
I also downloaded Pspice for TI, to verify the same.
However, I had different issue there.. It is not switching during normal working condition.. The G-E voltage is maintained at 12 V constant.
I would be obliged if one of your Engineer could contact me soon.
Thanks
Venkatesh