I am designing a controller card using LM3466 (or any other suitable IC) to balance the current for 15 arrays of 44 LED in each array. The Forward voltage is 3.1V to 3.4V. So in total 3.4 x44= 149.6V (maximum). We are using Constant current source power supply (limited to 2.1A). From the datasheet, it is recommended to use External MosFET circuit. (Please refer to the below image). But I could not able to find any suitable part number for the MosFet and resistor values. Can you please guide me with some recommended part number/resistor values based on my requirement. Thanks.