Hi,
Good day. I hope you are doing fine.
Our customer wants to use the LMR36015-Q1 in their ECU and he has a question regarding the inductor value for his design. They intend to use this to step down the 24V to 12V/1.5A, 400kHz. On the datasheet, table 3, they noticed that the suggested inductor is 27uH however they want to know if they can use a 22uH or 33uH inductor for this application as this is readily available on their inventory. Furthermore, they want to know the risk/effect of using the 22uH or 33uH inductor on their circuit. If this is possible, which one would be better in their target application.
Looking forward to your response. Stay safe and have a great day.
Regards,
Cedrick