Other Parts Discussed in Thread: TLV2711, TPS65130
Hello. I wish to power the TLV2711 low power Op Amp, supplying ±5V.
When testing with my prototype, I used the USB 5V and LM2664M6X to create -5V.
Now, I have to use a LiPo 3.7V with 200mAh battery instead.
Considering the power consumption and the IC size, is there a dual output device providing ±5V to power the TLV2711 from TI?
The input will be the LiPo 3.7V. Thanks for your kind help.