Other Parts Discussed in Thread: TPS709
Hi,
I am using TPS70912QDBVRQ1 IC for converting 18V to 1.2V output. Output load is 10mA worst case.
When I am doing HALT temperature on board. I Observed output voltage is keep increasing with increase in temperature. Could you please clarify what could be the reason.
Output voltage went up to 1.23VDC at 93 deg C ambient temperature.
Output capacitor : 10uF (C1210 package) , 0,1uF (Ceramic)
Input capacitor: 10uF (C1210 package) , 0.1uF (Ceramic)
Thanks
Ganapathi