Hello,
I am developing an ac/dc converter using UCC28250.
It is used as secondary side control, and the topology applies full bridge.
I am developing 3kW, and even if I load only 0.1A,
the heat rises close to 70 degrees in the UCC28250.
Even if you apply a little more load, the temperature continues to rise.
Other peripheral devices are fine, but only UCC28250 generates heat.
In case of no load, no heat is produced.
Which part should be reviewed?
Best Regards
Kwangwoon