This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS56221: Low current max.

Part Number: TPS56221

When i try use a circuit i got from the WEBENCH that is supposed to able to source 25A the maximum current i can get is 500mA.  

Design ID: 11
Part Number: TPS56221DQPR
Design Name: TPS56221DQPR 5V-5V to 1.50V @ 25A
The ouput voltage is correct but the current is low.
Thank you.