Hi,
in the datasheet it says the current from EN is either 1uA or 4uA, so it would never exceed the maximum value, right?
Are there any case that current of EN pin would be bigger than 4uA?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
in the datasheet it says the current from EN is either 1uA or 4uA, so it would never exceed the maximum value, right?
Are there any case that current of EN pin would be bigger than 4uA?
Hi Howard,
4uA is typical value at 'Enable threshold + 50 mV condition', the maximum value should be larger than 4uA.
Vincent,
thanks.
So EN current is only related to the device itself, right?
It's not possible that we design this circuit wrong and then cause the current becomes bigger, right? Then we don't have to worry about the probability that EN current may exceeds the maximum rating.
Hi Howard,
Yes the EN current is only related to the device it self. Changing the external resistors won't cause the current becomes bigger.