Hi Team,
My customer is designing LM76002 in his SCH and run a WEBENCH simulation which shows the recommended inductance is 15uH based on VIn=10V~36V, Vout=5V, Iout=2.5A, Fsw=500KHz.
https://webench.ti.com/power-designer/switching-regulator/customize/761?VinMin=10&VinMax=36&O1V=5&O1I=2.5&base_pn=LM76002&AppType=None&Flavor=None&op_TA=30&origin=pf_panel&lang_chosen=en-US&optfactor=3&Topology=Buck&flavor=None&VoltageOption=None
But in datasheet, recommended inductance is 6.8uF.
1. Is it OK if customer choose 6.8uH inductor in his application?
2. Why the simulation result is difference from datasheet's suggested value?
Thanks a lot.
Vincent Chen