Other Parts Discussed in Thread: UCC27517
HI,
I'm looking for a single drive IC that can drive the gates of MOSFETs in boost chopper circuits used in PFC circuits.
As a condition
・Pulse signal voltage input to the device : 5V
・Device Vcc: 12V ⇒ Drive MOSFET with 12V pulse from device output
・No other functions required
・Cost-oriented
・Insulation is provided separately
I think UCC27516 is applicable, but are there any other recommended devices?
(PFC circuit specifications)
VIN : 100V-240V
OUT : 390V 300W
Best regards,