This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
TPS650942 test cannot be turned on at -40°C Cold Start
PCH_PWROK (pin27) will be pulled off during the boot sequence
At that time, S0, S3, S4 and PMIC enable had no effect(Maintain at high level)
Question:
1.Can this operating temperature be -40C Cold Start?
Hello,
Yes, the TPS65094 family supports -40 C operating conditions.
Is the issue occurring on every board?
I would recommend taking a series of scope shots of the power up sequence (Figure 6-7 in the datasheet) to try to identify if there is a point where the power up sequence is not successful.
Hi Kevin
Thank you for your suggestion
Currently 5pcs is verified, the same situation will happen to 2pcs
Among them, 1pcs TPS650942, -40 degrees does not turn on and can be turned on after interchangeable