Other Parts Discussed in Thread: TPS2121
I am having some issues understanding how to set up the TPS2124 to switch between 2 supplies based on voltage levels.
I reviewed the documentation and I did not see anything that helps describe how to set the IN1 and IN2 levels for switching.
I assume it has to do with the PR1 input but do not see how to set this level for desired function.
Here is what my intent was for the IC when I first reviewed the data sheet.
Conditions:
12V into IN1
4.5V into IN2
Out set to IN1 (12V) initially
On loss of In1 (12V) to say less than 6V or lower, the OUTPUT switches over to IN2 (4.5V).
If IN1 increases to something > 6V the OUTPUT switches back to IN1.
How do I set the voltage that determines when IN1 switches to IN2 and back IN2 to IN1.
I understand the OVP requirements but not sure how to set these switch points.