Hi team,
Can you comment on the customer inquiry below, please?
In the data sheet of the controller, diagrams (Figures 4, 5 and 6) are shown on page 7, which include the short-circuit current. In the specifications you will also find the following information:
Now the question arises how the controller behaves when the output voltage is short-circuited (for example, via the output capacitor). Does a short-circuit current flow permanently? Is the short-circuit current limited at 350mA when the input voltage is 6V and the output voltage is 3.3V?
Maybe you can give me more information about the behavior of the controller during a short circuit?
Thank you,
Franz