Hey,
We are using the TPS22910 in one of our prototypes. We received 4 boards on which one has the TPS2991 rotated by 90 degrees.
We tested with the other board and the component works fine. For further testing it could work for us to simply bypass the device, but i'm not sure what will happen.
So the component is rotated 90 degrees, meaning that the:
Vin pin is now on the "ON" location
ON pin is now on the "GND" location
GND pin is now on the VOUT location
VOUT pin is now on the VIN location.
To bypass the device i'm thinking to basically make a link between the original VOUT and VIN location. What will happen with the device? will this create a short to GND somewhere?
Ofcourse sending back to my supplier and let them fix it is better, but i don't have time for that nor do we have the tools to repair it ourselves, unfortunately.
Kind regards,
Rob