Hello,
I have recently posted about an issue with the BQ24650 chip in supplying a continuous load while charging from a solar panel here: e2e.ti.com/.../945377. I have designed a battery protection circuit with an FS8205 MOSFET and DW01+G protection chip to prevent my battery from completely being depleted and triggering a cutoff. The design will however gives me the same issues with my protection circuit being connected to the VBat output (found below). Once my battery runs out of charge as providing a load of a low power MCU and step up converter, could it be causing a large voltage drop at the output of the BQ24650 chip and thus triggering the built in precharge timer??
Note: The overdischarge protection voltage is at 2.4V and its release voltage is 3.0V.
Here is the battery protection schematic & charging board schematic for reference:
And here are the datasheets of the components used:
FS8205 dual channel MOSFET: 
FS312F-G DW01+G Battery protection IC: 
Thank you!