This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM61460EVM: Question about external component

Part Number: LM61460EVM
Other Parts Discussed in Thread: LM61460-Q1,

Hello Team,

I have some questions about LM61460-Q1 EVM.

Q. Regarding with RBOOT resistor, I think adding RBOOT resistor decrease the FET turn on slew rate, then the noise will become small. On the other hand, Adding snubber circuit will also improve the noise performance. Do you know how effective are the RBOOT resistor and Snubber circuit respectively? OR is there any noise data when adding RBOOT resistor or when adding snubber circuit. Customer doesn't want to add snubber circuit if possible. This is because the snubber capacitor short may cause failure. So Customer want to know how much the RBOOT resistor is effective for increasing noise performance. 

Q. The LM61460EVM using 4.7uH winding inductor for L1. But customer want to use multilayer inductor for downsizing. Problem is that they can't find the multilayer inductor which has 4.7uH, 4A> rated current in the market. So they will plan to choice 1.5uH, 4A> rated current inductor for L1. In that case, is there any problem to affect the output stability or oscillation?

Thanks,

Yuta Kurimoto