My design specification is: 5V input, 3.3V output, load typically in the range 350 to 400mA. Schematic as below.
I have this working on a number of boards, no problem. However on one specific board, the SW output never starts switching; the output goes to about 2.70V. I'm powering the 5V input from a bench supply which shows input current of 197mA, so well inside the LMR14010's current / power rating.
Here are some turn-on waveforms. Yellow = 3V3 output, blue = SW output.
I've tried swapping the chip (twice) and the CB capacitor. I've also linked the 3V3 output from a good working board to 3V3 on the non-working (otherwise unpowered) board, so the good board is actually powering two loads. This works ok.
For reference, here are the corresponding waveforms on a good board (note the change of CH2 vertical scale).
Although this only happens on one board, I'm concerned that I might have a marginal design. Any suggestions / help very welcome.