This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM3421: LM3421 low ripple current

Part Number: LM3421

dear

    If there have LM3421 low ripple current sulotion such as sch or calculated inductance excel?  performace details show as below:

         Input above 48V, output 43V, average current 3A, ripple current maximum plus or minus 200mA,  thanks in advance