This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24650: BQ24650 circuit not charging Battery

Part Number: BQ24650

Please see the schematic screenshot attached.

Vin: 12V (DC Adapter) or 5.0V coming from USB

Vbat: 3.7V lipo (4.2V max charging voltage)

Measured:

Vref: 3.3V

Vcc: 12/5V

MPPSET: 1.2 (with a 5V source), 2.94V with a 12V source

TS: 1.6V and 2.19 V (tried 2 different R67 values)

LODRV has pwm pulses

V-regn : 6.0v (with a 12V source), otherwise 5.0 with a 5V source

Vfb: 1.95V (Vbat = 3.93V), charge termination voltage set at 4.1V

The stat1 pin is pulled low (LED on) while stat2 pin is high indicating that charging is in progress but the Vbat remains at battery level and battery never charges. I am not sure what I am missing or doing wrong.

Please help me identify the issue.

Thanks in advance.

Noaman

PH Pin waveform:

LoDRV pin waveform: