We have a board that uses 24VDC nominal and produces 3.8V. The initial load is very low ~3.3mA.
During initial test used a lab power supply to feed VIN started at 10V and increment. At around 20V the current increases again.
Using the lab supply meter at 20V is 25mA, at 24V is 50mA.
If we increment the voltage very slowly from 23V to 25V the current drops from 60mA to 15mA.
After this is done on every board, the slow voltage increment, the board will behave as expected, higher voltage under the same load lower current.
We have tried this on 8 different boards so far.
Thanks for your help
Carlos Weill