Hi,
- I'm designing a PoE device that should be powered either by the PoE connector or a DC adaptor (prefer 12V)
- The required output DC voltage is 5V (VDD of my system).
- For this I picked TPS2375 and I'm following the reference design: tidubr9 https://www.ti.com/lit/ug/tidubr9/tidubr9.pdf
In the Application note, it implements the adaptor ORing at the PoE rails, and it says the adaptor can be 12V. Meanwhile, in the application report SLVA306A https://www.ti.com/lit/an/slva306a/slva306a.pdf , it says Option 1 requires 48V at the top of page 3.
Question 1: Is a 12V adaptor sufficient to give the 5V at the output or not? Is there design change from tidubr9? I noticed RAPD1 and RAPD2 values don't match 12V (following the detailed design procedure in SLVA305C https://www.ti.com/lit/an/slva305c/slva305c.pdf )
Question 2: Can I power Up (start) the system by the DC adaptor (without PoE inserted) and vice versa? or does the PoE has to be there at first and then switch to the adaptor?