Other Parts Discussed in Thread: LM76005
Dear,
Our customer is searching a device of the following spec.
Would you please advise tell me the right device?
Vin 3.3~5V
Vout 30V
Iout 0.5(max)A
Best Regards,
Seijiro Matsuoka
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Seijiro:
Is it positive Vout?
I just curious why you put LMR70503
Minqiu-san,
Thank you for quick reply.
I'm sorry I had typo.
The following is correct.
Vin 3.3~5V
Vout -30V
Iout 0.5(max)A
Best Regards,
Seijiro Matsuoka
Hi Seijiro:
Never mind, just for confirm...The Vout is too large for LMR70503, I will suggest you use a Buck converter.
Here is an AN about that. https://www.ti.com/lit/an/snva022e/snva022e.pdf
Seijiro,
To get a non-isolated negative output voltage from a positive input voltage you would have to configure Inverting buck-boost topology.
See appnote: https://www.ti.com/lit/an/slyt286/slyt286.pdf
For 5V to -30V the SW voltage would be VIN-VOUT = 5-(-30)= 35V, so you would need at least a 40V device for this.
The duty cycle is D = VOUT/(VOUT-VIN), (-30)/(-35) = 0.86.
Also, the inductor current IL_avg = IOUT/(1-D).
At 5V the SW current would be 4.5A and at 3.3V it works out to ~5A, so you need at least a 5A device.
I think the LM76005 in inverting buck boost would be the best converter for this, LM76005 does not have inverting-buck boost WEBENCH model yet, but it should work.
I suggest you start a related thread specific to operating LM76005 in inverting buck-boost, you can link this thread for reference.
Thanks,
-Orlando