Hello Guys,
Good day.
Just like to confirm the following regarding the DC-DC converter of BQ25015:
1) If I connect the input to a 5V USB source, then the charge process will be enabled. I´d like to know what happens with the DC/DC down converter when this input has no power, i.e., when the USB source is not connected to it. Will the down converter work?
2) When I remove the USB power, will the DC/DC converter continue working with the battery connected as the chip enters in sleep mode ?
Thanks for the clarification!
Art